ALWAYS DOWNLOAD THE LATEST VERSION OF REVIT CONTENT BEFORE USING THEM IN A NEW PROJECT.

This change history file can be used to help you determine whether or not the changes
in the latest version available warrant the effort to update a family that is already
being used in an existing project.


Family File Dates: 2016 January 20
  - Added 350 ton size


Family File Dates: 2014 July 24
  - Released WMC-C's vintages


Family File Dates: 2013 October 1
  - Rebranded to Daikin Applied


Family file Dates:  2012 April 17
  - Added URL Parts Catalog

Family file Dates:  2011 October 6
  - Updated two URL's (Product Documentation Link and Product Page)


Family file Dates:  2011 Setember 15
  - Released all configurations of 145S, 145D, 150D, 250D, 290D and 400D models in single point power and multi point power


Family file Dates:  2010 Setember 10
  - Further reduced nested family usage and simplified geometry to decrease the file sizes even more
  - Assembly Code values are now compliant with MasterFormat 2010 (can be helpful for e-SPECS users)



Family File Dates: 2010 May 21

  - Upgraded to Revit 2010 format.  Changes include:
    - OmniClass value added
    - Defined exactly one type in the family, to help indicated if the Type Catalog wasnt used properly:
            "INVALID TYPE - Use Load Family and Type Catalog Instead"
    - Clearance volume changed to green (easier to see in Revit interference checks)
    - Set materials "Render Appearance" settings to create better images when the model is rendered
    - Material names better conform to the Revit Model Content Style Guide
    - Product Page URL parameter added for conformance to the Revit Model Content Style Guide
    - "URL" parameter value conforms better to Revit Model Content Style Guide 
    - To reduce load on Revit, web link parameters were changed to Type parameters
    - To improve usage for system design purposes, parameters such as those for capacities, temperatures, power values and others were changed to Instance parameters